Hi ,
My first post on a TI forum! Woot! Woot!
I am working with the LM2903 as a comparator in a discrete circuit, to perform a relatively simple operation, a simple circuit:
- It senses the voltage on the line on the (+) input, and compares it to a steady voltage on the (-) input (the comparing voltage), with NO feedback, and merely switches the output to be in 1 of 2 states : either Hi-Z output state or to GND output state. The output pin of the comparator has a pull-up resistor to some voltage, V_PULL_UP.
I was testing this in the lab, applying a variable DC source on the (+) line, and changing it to just confirm the two output possibilities. There is a transition region between the two outputs, where the output voltage is between GND and the V_PULL_UP votlage.
The range of transition voltages is very small, a fraction of a voltage. I was commenting, that this seemed normal in my experience. However, there was another engineer present, who was of the opinion, that was out of normal behavior.
I tried to take a look at the datasheet for the LM2903, but could not quickly located a metric to describe this transition range.
Can anyone comment on this? Any ideas? Thanks for your time!
Regards,
Evie
I think this is normal. The transition region is very small, a fraction of a voltage. However, there was another engineer, that thought this was not a good characteristic.