Hi all,
I have implemented a TLV3011 comparator as described below
That said, I am a little bit worried about the high current that would flow from Cp capacitor (10µF for the current design but could go over 50µF) to the TLV3011 output when the output goes to low state.
I read in the datasheet that the output is "short-circuit to ground" tolerant but I presume that only concerns the TLV3012 part.
Could you tell if this high capacitance output would be armufull for the comparator, even if the high to low state should occur about one a day in ower system ?
Or I need to add a limiting resistor between comparator output and Cp capacitor ?
Thank you in advance for your answer.
Best Regards,
Jean-Baptiste Osmont