I'm interested in using the OPA192. My input signal is a square wave, 0V to 2.5V, with a width/duration of 0.1ms to 10ms. The OPA192 will be configured so that it outputs a constant current output (load will be in parallel with the feedback resistor).
My question is, the OPA192 has a high output impedance - about 400 ohms in the range that I will be operating in. Does the OpAmp compensate for the high output impedance internally, or do I have to take the voltage drop into account? Example: 36V Vs rail, output resistance is 1000 ohms, the OPA192 output 30V, but only deliver 21V ? And if the OPA192 doesn't compensate for the voltage drop, is the output voltage range really only -500mV from the positive rail?
Also, there is a graph for Vout (V-) vs Iout, but not for Vout (V+) vs Iout. Why is that? Is there data for Vout (V+) vs Iout?
Thank you.