TL074's supply voltage timing is "Vcc+:15V → 5ms delay → Vcc-:-15V" because of customer reason.
Is it no problem?
Is there problem and inprovement point, please let me know.
Concern point is below.
・Common Mode Input Votage Range:±11V_min,
When supply only Vcc+:15V, Input voltage range is 4V~11V.
I think that TL074 will error on VIN:0V.
・In the past, the other OPAMP used only Vcc+:15V,
VIN:0V supply became nearly -15V.
I worry about whether the same thing will happen.
Best regards,
Satoshi