My OPA548 power amp circuit is not fully turning off when the chip is disabled. The output is pulling down to the -Vneg supply when disabled, when enabled, it works properly. I have dual +/-7.5V supplies and I use an open collector transistor to -7.5V on the E/S pin to disable the amp as shown in your appnote. Using a pullup to ground (0V) on the disabled output, I am able to pull the voltage closer to ground. With 1k to ground on the output, the output voltage goes from -7.5V to ~-1.5 volts indicating about 1.5mA of pulldown (leakage?) current. QUESTION: IS THIS EXPECTED? The amp text says pulling E/S down to -VNEG=-7.5V will disconnect the output from the load, but I am still seeing current flow thru the lower transistor to -VNEG??
Is there a way to FULLY turn off the output driver transistors when disabled?
Thanks