Hi,
Customer is considering OPA171. Could the device assured Vo=35V at Vin=36V and ILOAD=3.5mA ?
Regarding the datasheet description, is the electrical characteristics surrounded by red assured Vs=2.7 to 36V ? or only Vs=5V ?
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kato-san,
The comments that I made regarding the OPA170 in the previous E2E message apply to the OPA171 as well. Datasheet Figure 9 does indicate that the OPA171 should be able to provide Vo > 35 V, with Vs = 36 V, and Io = 3.5 mA. But keep in mind that the graphs indicate "Typical" performances and that are not specific assurances.
Under the "Electrical Characteristics" table heading it lists, TA = 25°C, VS = 2.7 to 36 V, VCM = VOUT = VS / 2, and RLOAD = 10 kΩ connected to VS / 2, unless otherwise noted. That would indicated that the Voltage Output Swing From The rail, over temperature, is over the wide Vs range.
Regards, Thomas
PA - Linear Applications Engineering