Hi
On the datasheet, it is mentioned as the following,
Signal input pins Voltage(2) (Vs-)-0.5V~(Vs+)+0.5V
Note (2) Input pins are diode-clamped to the power-supply rails.Input signals that can swing more than 0.5 V beyond the supply rails must be current limited to 10 mA or less.
1. How much it can be input more than 0.5V beyond the supply rail if the current is limited to 10mA or less? (0.7V? or more?)
2. How about negative rail? Is it possible to input more than -0.5V beyond supply rail if it is limited to 10mA or less?
Regards,
Koji Hamamoto