Hi,
I am using an LM258 in a simple unity gain configuration. Vs is 12V. V- is tied to Vout, and a voltage divider signal is input to V+. The signal itself is from a probe in a pull up configuration - pull up resistance is 1Mohm to a 1V supply, and when a contact is made to ground on the low side, the path is also about 1Mohm (through a low conductance fluid). Ground is common.
Most of the time this circuit works fine, but on occasion, the V+ pin will go to about Vs, which is 12V. This then produces and output of about Vs. This has happened on more than one chip. If I disconnect the signal input, V- stays high. If I power cycle the circuit, things go back to normal for a time, and then at some seemingly random point in the future, the same thing will happen.
Only one side of the chip is used. Do I need to ground the pins on the unused op-amp? I do not have decoupling caps, as we are just using this a crude threshold trigger, so we are not overly concerned with noise. Could some sort of power spike have damaged the circuit to cause this intermittent problem? Could it be a heat issue (circuit is in an enclosed space that gets warm (30-40C?). I wasn't sure if this was a known issue, or if some of the above precautions would make it go away. Thanks in advance for any responses.