Hi Bro,
One of my customer tested our TL084I thermal performance and found that: 20℃ temp increase at Ambient temp 25℃.
In their product standard, the max working temp is 70℃ which means IC is 90℃.
From TL084I datasheet, the max ambient temp is 85℃. Because the critical factor affecting device reliability and functionality is the junction temperature, but we only have RθJA=97 which cannot calculate the junction temp. So the question is how can we calculate TL084I temp? In addition 90℃ is higher than 85℃, does this has any risk?
Finally, we only found one 150 ℃ junction temp in the datasheet. So all the junction temp of TL084X are 150℃?
Thanks.