Hi Team,
The customer is using LF356MX/NOPB. In the data sheet, The "6.3 Recommended Operating Conditions" shows the supply voltage for LM35X is +-15V. And the
value is the max value. But there is not the min value. The customer has two issues.
Q1: Should LF356MX/NOPB refer to LF35x specifications?
Q2: Can we only use +/-15 V for the supply voltage? Or below +/-15 V can work normally? For example, +/-12V and +/-5V. That is if there is the the min supply voltage value for LF356.
Thanks,
Best Regards,