Hello,
We are currently using Divider IC MPY100AG in our existing board. But, this IC seems to be Obsolete
Chosen MPY634KP as an alternate
In our circuit, We are going to use the IC MPY634KP as Divider.
In EOL IC MPY100AG, there is an Offset Input VOS. But, this input was not there in the alternate MPY634KP. Will there any effect because of missing VOS in IC MPY634KP ?
Scale Factor : Our Input values - Numerator value in the range of -10V to 10V & denominator value in the range of 0 to +10V. Also, denominator value is always more comparing to numerator.
Due to this, We left scale factor Input as free (Not connected).
Divider Implementation in our circuit :
Inputs Signals connected to X1 & Z2.
X2, Y1 & Z1 are grounded.
Y2 connected with OUT pin
SF – Not connected
Is this connection valid to use MPY634KP as Divider using above inputs ?
Regards
Vinoth