Page 3 of the spec shows that I should connect pins 1 and 4 and 5 to V- but the note on page 17 recommends not to.
It vaguely states that it will result in a performance reduction. What does that mean?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Page 3 of the spec shows that I should connect pins 1 and 4 and 5 to V- but the note on page 17 recommends not to.
It vaguely states that it will result in a performance reduction. What does that mean?
Hi Mark,
The OPA551 pins 1,4 and 5 connect internal to the metal package leadframe. Each of these pin's connection point are at different corners. The reason pin 4 is specified as the primary current carrier on Pg. 17 has to do with directing current flow out through this pin which appears to produce optimum performance. If pins 1 and 5 are connected to a separate, floating copper thermal mass, then the primary current can't flow through them and it is forced to flow through the pin 4 connection.
Although I can't find anything specific about the mentioned performance reduction, I suspect it is with regard to the op amp's distortion performance. I wouldn't expect much of a change in it if pins 1,4 and 5 are connected together as Fig. 34 shows.
Regards, Thomas
PA - Linear Applications Engineering