Hello E2E, I am planning to use OPA454 to simulate 0 to +40VDC, I am going to make the op amp to have gain of 4 and input 0-+10VDC. I want to verify with you how low V- should be, because the datasheet doesn't say much about V-. For the simplicity of my work, I want to just tie V- to ground, but I am also afraid that would not allow me to have 0V at the output of the op amp. On page 6, it says that the output voltage can swing from V- to +1 or +2V. With V- tied to GND, would I expect around 1V on the output at Vin = 0V?
Thanks!
Russell