Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
Hi,
I am trying to design a howland current pump to feed an induction coil (inductance not known, resistance .25 Ohms). The output current have to be 2.5 Amps (peak), the voltage amplitude and shape is irrelevant as long as the shape of the current is sinusoidal. The input voltage signal is 2.5 V (peak to peak) Sinusoidal. The following design full fills the requirement regarding the current but only at low frequency i.e upto 150 Hz.
How can I modify the design to get the same output (2.5 Amps peak) for the same input (2.5 V peak to peak) but at higher frequency let's say 50KHz