Other Parts Discussed in Thread: TL974
Hallo support-crew and readers,
the following lowpass filter was designed with FilterPro and is used for pwm filtering:
We never had any problems while we used TL084CD operational amplifier. The filter response was excellent and never unstable!
But if we put TL084ID in the circuit the second stage becomes unstable and is oscillating with about 4 kHz.
The question is: Why does TL084CD is working very well but TL084ID does not?
Which op parameter does influence or explain this behaviour?
Is there a possibility to bring this circuit to work with both types of TL084?
Your support is very appreciated.