we are using this OPAMP for Sensing applications, please find below circuit, the Op-Amp giving continuously giving floating values when no probe is inserted, not sure why this happening, can you please check and suggest.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
we are using this OPAMP for Sensing applications, please find below circuit, the Op-Amp giving continuously giving floating values when no probe is inserted, not sure why this happening, can you please check and suggest.
Nagaraju,
What is the supply voltage at pins 4 and 11?
The input voltage should be 2V less than VCC for all temperatures and 1.5V less than VCC at room temperature, 25C.