Other Parts Discussed in Thread: TIPD120
Hi,
I'm required to design a voltage to current converter with the following characteristics:
- Grounded load
- DC current: ~1.5A
- AC current component: ~0.2Ap-p.
- Bandwidth: ~5MHz.
I was looking TIPD102 reference design.
Some questions:
- The implementation uses 2 stages in order to "allow the high side current source to accept a ground referenced input". Can you please elaborate regarding this consideration? Why isn't it sufficient to provide Vin at the input of the second opamp (i.e. removing the first stage)? Is the concern about ripple on the supplies that will directly appear on the output current?
- Is it a good topology for these requirements?
- Which modifications are required to make this circuit support 5MHz bandwidth and 1.7A current?
Thanks,
David.