This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM2904: Vcc Absolute Maximum Ratings

Part Number: LM2904

Hi all,

The absolute maximum rating of VCC is stated as ± 13 or 26 V in the data sheet.

My customer want to use Vcc=3.3V,GND=-15V.

If there is a problem please tell me why there is a problem.

Vcc-GND=3.3-(-15)=18 < 26.

Best Regards
Koji Hayashi

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.