Hi,
As per data sheet of LM339, the input voltage range is from -0.3V to 36V. We are using LM339 as a Comparator in our circuit , in certain cases, we have a voltage of -0.7V at Vin ( inverting). which is above the specification. Will it cause damage to Opam? What will be the behavior of Opam in this case? VCC is +24V and GND.