We are using a LM358 as a voltage-follower with an RC low-pass filter on the input to a 0-5V light sensor signal. The signal has significant 100kHz noise from the electronic ballast. Currently, R = 100k ohm, C = 0.1uF. What is the max value we can safely use for R without causing issues?