Hi,
I am a Doctoral student and working on Human Bio Sensors. The sensor is converting body temperature in to an Electrical Signal (DC Voltages). The range of DC voltages is between 2 - 5 mV with 1 nW of Power. I have to amplify these voltages to 3 V. Is there any amplifier which can solve my purpose ?
In addition, the output voltages are not PURE DC. There are probably AC components. So what other component I require to get Pure DC Amplified Voltages at the output ?
Thanking you in anticipation.
Best Regards,
Ahsan