This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL074: Output status for no input signal

Guru 19485 points
Part Number: TL074
Other Parts Discussed in Thread: TINA-TI

If in the case of Vcc+: +15V / Vcc-: -15V / Input: 0V, can TL074 output keep 0V? 

I hope to keep Vout: 0V, but TINA-TI result was 2.54Vout.

I want to confirm Vout is 0V or not for above condition.

If not, is there countermeasure the external circuit? 

Best regards,

Satoshi