This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE031: AFE031

Part Number: AFE031
Other Parts Discussed in Thread: AFE032

Hello,

PA of AfE031 doesn't provide me the calculated amount of current(1.6A),the external ISET resistor  connected to  PA_ISET pin (pin 46) is 10K,but the maximum output current of the power amplifier i get is 1A, i expect 1.6A, what is wrong?

Kind Regards!