This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMC6492: Need a current pumping /boosting/amplifier for battery charger

Part Number: LMC6492

Hello Sir,

My application need a battery management charger IC.
Take a look the design layout,



1. A micro USB connector from smart phone to PC or power adapter will be use.
2. From this USB connector VBUS will be supply power to my external system through the battery charging IC.
3. This IC will manage the 5V , 2A power from adapter but, in quick charging mode, 9V, 2A power should be block by the management IC.

If you look on the diagram you would see, the current path is divided in 2 ways!

In QC mode, the adapter has 9v/1.67A, after connected the Galaxy note 5 we saw 1.23A is operating.

Right at the moment, we have faced a problem that is the charger ic side current will be 0.44A to 0.30A( depending on the supply current from adapter or over voltage and current protection).

The battery we gonna use has 3.7V 2200mAh in actual spec capacity. (sorry for my previous information)
It will take long time to charge the battery

I think we need to boost up the current level more, I am not sure what would be its value.

Can I use  Howland Current Pump in this purpose? www.ti.com/.../snoa474a.pdf

If you have any idea about this solution, let me know please.

HW Engineer

Hasan

  • Hasan,

    Trying to force more current into VBUS than VBUS wants to draw will only cause VBUS to increase in voltage. Higher voltage is not good for the system. If you get 9V to the Note 5 (after it asks for it) and it draws 1.23A instead of 1.67 Amp then that is the Note 5's fault.

    The Howland is for linear signal processing and isn't an efficient way to supply current in a power supply application.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

  • In reply to Ron Michallick:

    Yes, I understand. The current falls due to impedance matching, and also not all time it provides 1.67.
    Anyway. we are using BQ24266 charger IC, lets see what happened after that.

    HW Engineer

    Hasan

  • In reply to MD MUBDIUL HASAN:

    Hasan,

    If you have any questions specific to the BQ24266 or any other charge supervisor, please start a new thread using that part number so the expert for that device will be notified to respond.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.