Other Parts Discussed in Thread: OPA548, OPA547
I am currently working on a design to generate a 5VAC (rms) @ 400Hz supply capable of 5A continuous. The design contains a non-inverting amplifier that takes a 213mV (rms) @ 400Hz voltage waveform (generated by a COTS board) and boosts it up to 5VAC (rms) @ 400Hz. The circuit is shown below:
This circuit works just fine, effectively generating the 5VAC (rms) output that I desire... that is... until I put it under load... When I connect this thing to our expected load (special incandescent aircraft light-bulb design, the voltage on the output waveform gets sucked down to 4.6VAC (rms) and draws 1.14 Amps AC (rms), and stays at 4.6VAC (rms) until I remove the load. When I remove the load, the amplifier output returns to 5VAC (rms) @ 400Hz. What could be causing the voltage to get sucked down like this?
Some additional information (not sure whether it will help anyone looking at this, but figured I'd share as much information as I actually understand/know). I've tried a specialized industrial supply capable of 5VAC @ 400Hz (at very high current) and the voltage does not get sucked down at all. Under normal circumstances the bulb draws 1.15 Amps AC (rms) from the industrial supply when 5VAC 400Hz is applied, not impacting the voltage whatsoever. I am convinced there is something wrong with my amplifier circuit...
Additionally, I am heatsinking this with a huge chunk of aluminum I found back in the shop. A thermal gun indicates that the actual part (not the heatsink) is at roughly 30 degrees C under these conditions.
Additionally the load is a string of incandescent bulbs in parallel, which are antiquated and thus I cannot provide specifications for. I estimate the load (based on measurements previously mentioned) size to be 4.4 Ohms.
Let me know if there are any other details that would help if I provided, or am missing something.