To whom it may concern I would like to ask for an OP V= +12 V , -V =-12V
1) We have to develop one-two analog channels Differential and single ended
a) Differential Input V = +-10V ,
b) Single Ended V= 0 to +10V
Our ADC convert is 16 SAR VCC= VADD = 3.3V, Could you suggest me an OP that can work for those Input Voltage ?
2) Also We need to create a DAC from 0 to +10 V , we would like to control different output signal from a PWM 16 bits, Vout = 0 to 3.3V .
THE DAC Output Voltage = 0 to +10V. Iout = 200 mA
Could you suggest me an OP rail to tail low offset for this application
Regards
Albert Tello