Other Parts Discussed in Thread: TLV3201
TLV3701QDBVRQ1 Comparator on +5V PSU is not working correctly, tested 3 of them which has strange output
Pin 4 (-VE) = +2.5V
Pin 3 (+VE) = +0.2V
I get 5V O/P which should be 0V !.
It toggles voltage but it appears to behave as an inverter. I checked datasheet and it not clear that it actually inverted O/P. I checked the IC marking which is in sync with TLV3701QDBVRQ1
I swapped with TLV3201AIDBVT and it worked correctly. It is SOT23-5 same package and pin layout.
Not sure what to do with TLV3701QDBVRQ1.....I have 7 out of 10 left (ordered from Mouser). Do you have a history of batch failure?
R.