Other Parts Discussed in Thread: TINA-TI, MSP430F5636, OPA196, DAC7811, DAC8811
Hi,
i wish to use the OPA454 as an non-inverter op-amp.
The input voltage coming from DAC (0V ~ 2.5V)
the gain in +40.
the supply voltage for V+ is 100V
the supply voltage for V- is 0V (GND)
I'm running the design with TINA-TI and for some reason I get this result:
but when I put the V+ to 95V and V- to (-)5V it work as expected:
So before i start the layout i would like to know if this device can be used for my application.
Thanks