Other Parts Discussed in Thread: TLV3201Hello John
good to see the list, it seems all of interest is there at least the model you refer to...
I do not see however this header in the model I've downloaded:
.SUBCKT TLV3201 3 4 5 2 1
M12 6 7 8 8 MCPO W=200U
M13 6 7 9 9 MCNO W=200U
E1 10 11 12 11 20
E2 11 13 14 13 0.5
R1 0 11 1E9
R2 0 11 1E9
C1 7 15 1.8E-12
R3 7 16 800
E3 15 13 6 13 1
........
It seems not each model contains the header, or?
Best regards
Ivan