Other Parts Discussed in Thread: OPA189, OPA2189, OPA454
Hi there:
I'd like to check whether it has OPA series could operate in ±2 V to ±20 V?
currently OPA2277 could operate in 18V max.
And the driving capability could up to 50mA or more?
Application would be 13~15" LCD panel T-con board used.