Hello everyone,
I am facing a problem for which I can't seem to find a solution.
I need to measure a current through a shunt resistor and current sensor amplifier, for which "standard" components and designs already exist at TI, but here's the catch :
-The amplifier is supposed to be supplied with a 3.3V supply
-The signal of which current will be measured has a common mode of maximum 40V (if the acceptable common-mode of the component is higher, it would be even better).
-Preferably the component should be Automotive-Grade, and with a 50:1 gain
I have identified devices such as the INA 282 Q1, the INA 148-Q1, the TSC1031 and the LMP8602Q1, but either information is lacking regarding the acceptable common-mode under a 3.3V supply, either it is given but too low for my application.
I may add that precision and speed of the measurement are not critical.
Would anyone have any advice regarding my issue ?
Thanks in advance,
L Perbet