Hi Teams,
My customers have questions on setting up VICR.
The following specifications are Min = 0 to Vcc - 1.5V at 25℃
For example, when Vcc = 2 V, the Min specification becomes 0 to 0.5 V, but at that time, VICR is 1 V.
Is this out of range?
Does the problem occur?
In full range, it is 0 to Vcc - 2V. Does temperature change affect both high temperature and low temperature?
Best Regards
Kenji
.