Other Parts Discussed in Thread: TINA-TI, TMP411
TI,
I have constructed a circuit using the OPA564. Everything appears to be working fine, thus far --- but I am trying to validate the correct behavior of IFLAG and TFLAG.
First, for TFLAG I want to verify the correct behavior when used in conjunction with the E/S pin.
- It appears that in my test circuit, TFLAG is high when E/S is pulled low (shutdown).
- It is also high when E/S is high or unconnected, but has gone into thermal shutdown.
Thus, is it true that TFLAG is high whenever the device is shutdown?
Second, for IFLAG I want to verify that the correct behavior when in operation, with ILIM resistor 54.9k, ( Sets current to 24000/(54900+5000) = 0.40066778 A )
- I cannot get the current to go over 0.300 A in the circuit when it is set in this way.
- In the same scenario, I am seeing an immediate drop toward 0 A the higher and higher I try to push the current after this threshold.
- I cannot trigger IFLAG for this reason.
- It is variable however, if I use 20k in parallel with the 54.9k for example ~14.66k = 1.22A it falls off right around 1.05A.
How can I trigger IFLAG without it 'pinching off' right before the value?
Worth noting is that I am using a level shifting circuit on BOTH outputs. they are identical. for both IFLAG and TFLAG.
Vdig is +4.3V and VCC is +5V in this scenario. V- is -6V and V+ is +6V
Thanks