Hi,
Our customer is evaluating INA826 at +12V / -5V power supply.
Is there a problem with this method?
I think no problem at general IN AMPs.
But, they are complaining that the power supply malfunctions when using the LTC1983-5 negative charge pump for the AD8221.
In this case, LTC1983-5 output dropped from -5V(nomal) to +0.5V.
They think AD8221 can't use unbalanced power supply.
This is a question that ADI should check, but it is an opportunity to replace it with INA826. I think that there is only INA826 because it is MSOP.
In the simple evaluation by the customer, the operation of the INA826 and the power supply IC is normal.
Is there a problem with INA826 with the following circuit and unbalanced power supply?
Because the temperature change of the forward drop voltage (VF) of the Schottky diode (RoHM / RB 060 MM - 60 TR) is unacceptable, the circuit that acquires and cancels the forward voltage with the instrumentation amplifier (G = 1) made up.
Therefore, the anode is connected to the noninverting input terminal (+) of the instrumentation amplifier and the cathode is connected to the inverting input terminal (-).
The problem occurs at power up, so the actual VF is nearly 0V.
I'm sorry for my strange question.
Best regards,
Hiroshi