This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Andrei,
Power operational amplifiers are commonly employed in TEC driver applications. A properly specified power op amp should provide very good performance in that type of application.
You mention a requirement for a voltage up to 10 V which I assume is the output voltage swing that is needed. Both the OPA567 and OPA569 are specified with a maximum operating voltage of +5.5 V, and wouldn't be able to support the 10 V output swing requirement. In order to swing the 10 V the power op amp would have to be powered by a supply greater than 10 V, and be capable of delivering the 10 V output swing at the required output current level.
Two power op amps that I think will cover your TEC application nicely are the OPA547 (0.5 Amp) and OPA564 (1.5 Amp). Both can deliver more than 200 mA, and having the higher output current capability allows their output to swing closer to the supply rails. You can find more information about the OPA547 and OPA564 in their datasheets found here:
TEC applications often use a bridge-tied load configuration as seen in the OPA567 datasheet Figure 14, or OPA569 datasheet Figure 20. Two OPA547 or OPA564 power op amps could be connected in the bridge-tied load circuit as well.
Regards, Thomas
Precision Amplifiers Applications Engineering