This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/LMV761: LMV761 Spice Model For Supplies between 2.7V and 5V

Part Number: LMV761
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hi,

I am working with the spice model for LMV761. According to the datasheet, recommended operating conditions for the supply are +2.7V to +5.25V, however electrical characteristics are given for +2.7V and +5V supplies only. Is the spice model defined for supply voltages between those values? My experimentation and some related posts suggest it may not be. If that is the case, is there an updated model available that is well behaved for supply voltages that are not 2.7V or 5V?

Thanks!