Other Parts Discussed in Thread: OPA177
Hi dear expert,
We met an issue when using INA128. Vs+=5V, Vs-=-5V, during the power supply ramps up, the input pin can be observed a negative voltage overshoot down to -1.7V and will ramp up very slowly to 0V, the ramp up time can last 2 seconds. Below snapshot is from input pin:
If we make Vs-=0V, the input pin will be not seen such a big negative voltage and the settling time is also shorter, around ~10ms. See below pic with VS-=0V.
The schematic is as below: INA128 is the middle device.
Our questions:
1. is this phenomenon is expected? and the input negative voltage is generated from INA128?
2. Is there any way to make the settling time shorter to xxms?
Thanks a lot for your reply.
Joyce