I am using the LM2907 in a frequency to voltage configuration. My input power supply varies from 23-26V, and it is causing too large of a swing in my output voltage.
I have decided to switch to the LM2917 part instead with the internally regulated supply rail of 7.56V, but I need to know the tolerance on this so I will know the tolerance on my output. I didn't find it in the datasheet, and I opened a case but they instructed me to come here.
I am planning on using a 2K current limiting resistor on pin 6 of the device from the supply rail. Not sure if that makes a difference.