Other Parts Discussed in Thread: DRV8701
Hi guys,
one of my customers is testing DRV8701EVM and wants to add an emergency stop. If they implement this by putting the device into sleep mode at very high load would this pose a risk of damaging the circuit? Would this be a risk if this would take place lots of times?
They also measured temperatures of the board and saw 48°C on the chip, when in standby at about 37V. Is there a specific reason for the temperature to be elevated and can it be decreased?
One more question: Is there a reason why the EVM is only available with the E version (without coasting) and not the P version (with coasting)?
Thank you,
Franz