This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

INA214-Q1: INA214's gain error when Vsense is over 5mv

Expert 4695 points

Replies: 1

Views: 88

Part Number: INA214-Q1

Hi expert,

I wonder how to get gain error data over the test condition of datasheet shown below for INA214:

I searched through the datasheet and didn't get much that helps. For example, how do I know the Gain error when Vsense is from -20mV to 20mV?

Thanks

Sheldon

  • Hello Sheldon,

    Gain error is consistent for different values of Vsense, as long as the device output is not saturated. We are not able to spec gain error at large Vsense values since we have some devices with gain as high as 500V/V or 1000V/V, which would saturate if we applied an input signal such as 20mV.

    Best regards,

    Ian Williams
    Applications Manager
    Current Sensing

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.