Hi,
In the user's guide I read :
"In four-wire module applications, it is essential that the OWD Bit (Register 4 [D15]) be set to '1' to disable the One-Wire interface after final programming is complete and before the final sensor module is sent out to the end application."
I already use a Pull-up on the PRG pin. Should I set this OWD bit to "1" in this case ? Because when I set OWD to "1" after calibration the sensor doesn't work (maybe due to this pull up)
Do you have some pieces of information ?
Thx
Guillaume