Other Parts Discussed in Thread: XTR117, XTR111, OPA188, OPA333, INA317, OPA227
My sensor gives out an AC signal at 60Hz up to 1V. I assume the XTR115 cannot use an AC signal directly (also because the circuit I built isn't working as it should) and by simulating the circuit in LTspice, I can't seem to use Vref to offset the AC signal to make it only in the positive range. I would prefer avoiding diode to rectify the signal but how can I offset the input AC signal to make it so the XTR115 can work properly?