Hi,
I plan to use 5962-9753702QHA and need to know the following:
- Are these cavity type parts?
- Do these parts require PIND screening?
Thank you,
HSG
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I plan to use 5962-9753702QHA and need to know the following:
Thank you,
HSG
HI,
The applications engineer supporting this device returns to the office on Wednesday. We will try to get answers to questions before then but responses could be delayed.
Thanks
This is a military grade product, so it will be in a hermetic package which has a cavity. Military grade products do not get 100% PIND. The requirement is a periodic PIND test on the package family.