Other Parts Discussed in Thread: THS4551
Hello,
I have an RF tuner with high impedance (2.2K) 1.0V PP (2.0V PP max) output at 700KHz ±100KHz, i need to drive the input of an STM32 12bit ADC. The tuner output is differential, the STM32 ADC input can be set as differential or single end. I also have a 4:1 transformer, which i would rather avoid to use since its expensive, large and space on PCB is sparse. I think the OPA365 could be used to scale the tuner output to the STM32 range (3.3V) and i would like to have suggestion on how to connect it and which values to use assuming the tuner output is set to 1.0V PP output.
Thanks