Could you please share the Output and Input Slew rates of TLV3201AIDBVR ?.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Prahlad
Comparators are specified in terms of output rise and fall time. In the case of the TLV3201, these are typically 5ns are refers to the 10% to 90% transition levels.
In regards to your input slew rate question, I am not exactly sure what you are seeking. The min pulse width at the input that we can expect to see changes at the comparator output is 2x the propagation delay (tplh + tphl).
Chuck
We have not seen any response on this thread for a while, so I will be closing the thread.
If you need further assistance, please feel free to reopen or start a new post.
Thanks
Chuck