Hi,
I don't know how to calculate current monitor chip SN1906023-Q1 itsself power dissipation. can you provide related method?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I don't know how to calculate current monitor chip SN1906023-Q1 itsself power dissipation. can you provide related method?
Hello user,
To calculate the power get the max IQ of the device and multiply by the VCC you are applying to the supply pin. If the output is driving a load you need to account for that current as well in the IQ. You should also use the maximum output current you are expecting.
Hi Javier
Thanks for your support.
This current sense output is connected to MCU two ADC pin for monitor, so as to calculate the power dissipation, current should be IQ+Iout_ADC?and Power dissipation=Vs*(IQ+Iout_ADC)?
Hello User,
That is correct. Normally the input to an ADC will be minimal and will not impact the power calculation much.