Other Parts Discussed in Thread: VFC32, , LM331
Hi,
I'm interested into use VCF320 as Fast-settling FVC.
In my application I've a square wave signal with an input frequency ranging from 1.3KHz to 4.8KHz, coming form a magnetic pick-up sensor. The VCF320 supply voltage is +-15V.
I want to reach a settling time of less than 1ms, to do this I chose the following components (refer to the SBVA005 application note):
R6=36.5kOhm 1%
C3=2.2nF 1% Polystyrene
C2=3300pF NPO ceramic
Are those componets corrects?
Also I have doubts in choosing the right S/H circuit for this application, what are the main constraints for S/H? Do you have any suggestions on modern components that can be used?
Thanks in advance.