Other Parts Discussed in Thread: TLV3701
Hi Team,
A customer of mine had the following question concerning the TLV1701.
The output of the TLV1701 requires a pull-up resistor. He was wondering what the max value of the pull-up resistor might be. The application is low speed (switching 2 times every 10ms) but also very low power.
Can a pull up resistor of a few 100kohm be used?
Or is is it better to use a comparator with push-pull output in this case?
Thanks in advance for the help!
Regards,
Obi.