Hi,
I am having trouble designing an amplifier circuit for a photo diode. I have very little light, so even with the best SiPN diodes, I only get about 500nA current from it.
The amplification also needs about 15MHz of bandwith. I would prefer to have an SNR of >100, meaning a noise level of maximum 45mV at the output signal.
I have +-5V available as well as an LDO solution for a selectable lower voltage.
Is there a suggestion for a solution that would be a best guess on how to solve this?
I have only done testing using a competitors amplifier, and I get 200mV of noise and ringings.
Thanks!