My project use DRV2605EVM-CT try to trigger vibrator.
I have some questions.
1. I use I2C to read Status (0x00) address, it return 0x60
In spec. I know this DRV2605 device.
but the source code (http://www.ti.com/lit/zip/sloc283) -> drv2605.h
#define DRV2605 (5 << 5)
#define DRV2604 (4 << 5)
define error ?
2. I just want use goip or GO register to trigger ERM vibrator on External or Internal Trigger Mode.
How many registers need to write ?
I try to write, but the vibrator can't work.
I2C Write 0x01 : 1
I2C Write 0x02 : 7f
I2C Write 0x03 : 0
I2C Write 0x04 : 8
I2C Write 0x05 : 8
I2C Write 0x06 : 8
I2C Write 0x07 : 8
I2C Write 0x08 : 8
I2C Write 0x09 : 8
I2C Write 0x0a : 8
I2C Write 0x0b : 8
I2C Write 0x0d : 0
I2C Write 0x0e : 0
I2C Write 0x0f : 0
I2C Write 0x10 : 0
I2C Write 0x11 : 5
I2C Write 0x12 : 19
I2C Write 0x13 : 64
I2C Write 0x14 : 19
I2C Write 0x15 : ff
I2C Write 0x16 : 90
I2C Write 0x17 : 90
I2C Write 0x18 : 14
I2C Write 0x19 : 72
I2C Write 0x1a : 26
I2C Write 0x1b : 97
I2C Write 0x1c : a5
I2C Write 0x1d : a0
I2C Write 0x1e : 20
I2C Write 0x0c : 1